Plug loads include devices connected to standard receptacles, such as task lighting, monitors, chargers, and other electronic equipment. Even when not actively in use, many of these devices continue to consume electricity through standby, or "vampire," loads. Plug load controls automatically shut off designated receptacles when spaces are unoccupied, helping reduce energy waste, lower operating costs, and improve building efficiency without impacting occupant comfort or behavior.
What are Plug Loads?
Terms to Know - Plug Load Control Fundamentals
|
Term |
Definition |
Why It Matters |
|---|---|---|
|
Plug Load |
Electricity used by devices plugged into receptacles, such as monitors, printers, chargers, coffee makers, and other equipment left in standby mode. |
Plug loads can account for a significant portion of a building's energy consumption. |
|
Plug Load Control |
A system that automatically turns receptacles on or off to reduce wasted energy. |
Helps customers save energy and meet energy code requirements. |
|
Energy Waste |
Electricity consumed when equipment is operating unnecessarily. |
Identifying waste creates opportunities for cost savings. |
|
Standby Power (aka Vampire Load, Phantom Load) |
The electricity used by devices when they are plugged in but not actively being used. |
These hidden energy costs add up over time, especially across large buildings with hundreds of devices. |
|
Energy Efficiency |
Using less energy to perform the same task. |
A key goal for most building owners and facility managers. |
|
Uncontrolled Receptacle |
An outlet that always remains energized. |
Critical devices should remain plugged into uncontrolled receptacles. |
|
Controlled Receptacle |
An outlet that can be automatically turned on or off by a control device. |
The core component of most plug load control solutions. |
|
Split Receptacle |
A receptacle where one outlet is controlled and the other remains always on. |
Provides flexibility for users. |
|
Occupancy-Based Plug Load Control |
Automatically energizes and de-energizes controlled receptacles based on occupancy. |
Prevents devices from turning on when no one is present. One of the most common plug load control triggers. |
|
Schedule-Based Plug Load Control |
Turns controlled receptacles on and off according to programmed schedules. |
Reduces after-hours energy consumption. Ideal for predictable operating hours. |
|
Automatic Shutoff |
Power is removed from a device after a programmed condition is met. |
Eliminates unnecessary energy waste. |
Codes and Standards
Energy codes and standards require Receptacle Control or Plug Load Control. IECC, ASHRAE 90.1 and California Title 24, Part 6 require controlled receptacles to have the same automatic shutoff function as lighting using either occupancy sensing or schedule-based control. Plug-in strips and devices cannot be used for code compliance. Title 24 and NEC also require the controlled receptacles to be permanently marked to differentiate them from uncontrolled receptacles.
Big Three Code Compliance
|
Requirement |
ASHRAE 90.1 2025 |
2024 IECC |
2025 California Title 24 |
|---|---|---|---|
|
Where Automatic Receptacle Control (aka Plug Load Control) is Required |
|
|
|
|
Number of Receptacles That Must Be Controlled |
|
|
|
|
Placement Requirement |
|
|
|
|
Allowed Control Methods |
|
|
|
|
Auto-OFF Timing |
|
|
|
|
Scheduled-based Control |
|
|
|
Controlled Receptacles
Plug Load Control Strategies
Occupancy-Based Plug Load Control
Plug load energy savings are achieved by de-energizing devices when not in use – often determined by whether someone is present.
- Occupancy sensors turn plug loads on when users are present and off when the space is vacant
- This targets one of the biggest sources of wasted energy – idle workstations
- High savings potential during both business and non-business hours
- Requires careful sensor placement and tuning for reliable performance
Design Tip
- Use in spaces with unpredictable occupancy like private offices, conference rooms, or classrooms
Scheduled-Based Plug Load Control
Time-of-day scheduling is ideal for spaces with predictable occupancy, like offices or classrooms.
- Receptacles turn off automatically after hours based on a preset schedule
- A manual override can keep outlets on for up to 2 hours, if needed
- A 24-hour holiday shutoff is required—countdown timers don’t qualify
Design Tip
- Use scheduling for core hours, and pair with occupancy sensors in less predictable spaces
Looking for ways to reduce plug load energy waste and comply with energy codes? Download the brochure to learn how Leviton Plug Load Control solutions can help.
Applications
Occupancy-Based Plug Load Control
See how automatic shutoff strategies are applied.
Scheduled-Based Plug Load Control
See how time-based schedules can reduce plug load energy waste.
Find the Right Plug Load Control Solution
How can we help you?
Speak to one of our Plug Load Control Specialists.